Hi all
Im using 3 solar panels in parallel, with approx 300ma generated peak current across the terminals (and 3.5v). However, when i connect that to the input of a TPS61220 boost module set for 5V, the output voltage is fine, but the output current is only approx 70ma.
What am I doing wrong or perhaps overlooking ?
(Using the standard circuit as in the datasheet, though with a 5.6uH,300ma chip inductor. This should not have any effect on the current drop theoretically)
Regards
Soumitra