We are using the TPS2590 in an application where the spread between I fault and I lim needs to be as small as possible. Page 7 of the data sheet warns that Ilim needs to be larger than Iflt even considering tolerances. Do these "tolerances" include the min to max range of Ilim and Iflt on page 3? In my calculations, do I need to use Iflt max and Ilim min or can I expect these values to move in the same direction? (i.e. if Iflt for the part is closer to the min, I can expect Ilim to be closer to it's min as well)