Other Parts Discussed in Thread: LM5118, LM2677
Hello all,
I am trying to figure out if the LM5118 will still work in my power board design. I already have the power board populated so if a change needs to be made I need to know about it asap since I am on a tight schedule.
Ok so I was using the LM5118 with an input voltage Vmin = 17.5 Vmax = 29.4 Vnom=25. This setup worked fine, I did not design it however. Now I need to up the input voltage to Vmin=25 Vmax=42 Vnom=36.
Iout = 5A.
Vout = 24V
VCCX = NONE
Switching Frequency = 300kHz
Ripple current as % of Max Load Current = 40%
TA = 25 degrees C
Can I still use this regulator? According to the spec sheet it should be able to handle any input up to 75V.
If you need more information just ask.
Thanks