Hi,
Can you please provide the following information for the TPS2491DGS part?
1. Junction Temperature Max (Tj Max)
2. Thermal Resistance Junction to Ambient (Theta JA)
Thanks in Advance
Dibin Mathew
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can you please provide the following information for the TPS2491DGS part?
1. Junction Temperature Max (Tj Max)
2. Thermal Resistance Junction to Ambient (Theta JA)
Thanks in Advance
Dibin Mathew
Maximum junction temperature is specified in the absolute maximum ratings table of the datasheet as 150C. There is also a dissipation ratings table in the datasheet which lists a derating factor (3.76mW/C) and several power dissipation ratings vs. temperature based on designing to the recommended operating maximum junction temperature of 125C. Use the derating factor for your thermal design to keep the junction below 125C.
Hi Eric,
Thanks for the reply.
I need to know the thermal resistance of TPS2491DGS. Can I take it as 266 degC/W (1/3.76mW/C).
Plz confirm.