This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40210 and inductive load

Other Parts Discussed in Thread: TPS40210

Hi everbody,

I want to use TPS40210 for my university project. I control four solenoid valves by PWM signal from uC. Problem is in that solenoids valve need 24V supply power @4A together but i have only 12V at the disposal. So my question is, Is TPS40210 good choice for this application? what configuration is most suitable? Entire load in one branch is cca 15mH with 50ohm in series,type of flyback diode is ss12 and PWM signal have 30kHz switching frequency. In advance thank you for all kind of reply.