Hi! I want to use the BQ24610 for following application:
We develop a High-Power LED Light which is powered by a 4-cell Lithium Polymer battery- pack. The battery-pack should be charged by a PoE DC/DC Controller which can deliver about 24W continuous. This power isn’t enough for the High-Power LED circuit, so i want to use the battery pack as a puffer…means the power for the LED circuit should be taken from the battery-pack all the time.
My question: Is it possible to design the BQ24610 circuit in such a way, that the power is always taken from the battery pack although the DC/DC Controller Voltage is higher than the battery voltage?
Meanwhile I don’t think so…so I have the following solution statement:
1.) DC/DC controller output voltage must be controlled, to simulate an absent “AC adapter”.
2.) Charging the battery-pack: Load is switched off; set CE-Pin HIGH to enable charge.
3.) SOC of battery-pack is near by 100%; set CE-Pin LOW; set “AC Adapter”-voltage 0V to supply the High-Power LED’s by the battery-pack.
In this case the battery-pack would be charged when the load is turned off and it is not possible to charge the battery-pack when the load is turned on….
I hope you guys have got my problem, I hope it is an error in reasoning … so is there any chance to use the battery pack as power supply all the time, whether the AC Adapter is plugged in or not?
Thanking you in anticipation,
Steve from Austria