This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SM72445 Circuit Question.

Other Parts Discussed in Thread: SM72445

Hello i'm trying to build the circuit showed on the datasheet of the SM72445 but i have the following questions:

1- If I set the pin A2 to 3.44 V to opperate in low frequency and to use the  H-bridge for PM operation. Does that means that the PM_OUT pin becomes useless and i can avoid using the whole circuit related to it? I mean the PM driver and the 2 Transistors?

2- Wich H-Bridge driver would yo recomend me to use? ir2110 is ok? Idon't know if i can use bootstrap because the high side of the bridge couln't opperate in ON state continuously.Could you suggest me a circuit?