We want to prevent charging of a pack if a cell under voltage is 2.0 volts or less. I see the CUV flag set in the Safety Status. It is not set in the Safety Alert. The pack is at rest drawing zero current. I can set the cell imbalance flag to blow the chemical fuse. I would like also prevent the pack from trying to charge the pack. because one or more cell are at 2.0 volts or less. Can I blow the chemical fuse under this condition?