This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

uc3843---Pin3 maximun rating

Other Parts Discussed in Thread: UC3843, UC3842

Dear,

our customer find there is a -1.2v nagtive voltage at Pin3 of uc3842 when perform the short circuit testing, as below picture however,the  Uc3843 datasheet show the maximum Pin3 rating is -0.3v to 6.3v, what 's the risk of the -.12v negtive  for the uc3843? i notice the pin3 is connecting to the minus input  of  amplifier, what's the consideration of 0.3v maximum rating  here?

 

 

  • Swing,

     

    We  cannot recommend that any customer should operate our parts outside their maximum ratings. In this instance less than -0.3V on pin3.

     

    Having said that please ensure that the customer is doing a tip and barrel measurement between pin 3 and pin 5 at the IC pins to see if the pulse in real. There was no picture attached to the post.

     

    Regards,

     

    Richard.