may i use LM2733 to implement a power of negative -12v input,positive output +3.3v?
if can,how to calculate the value of R18 & R19?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Alan,
it could work but you have to use a zener diode in series with the VIN pin.That is needed since the maximum voltage on the VIN is 14V to GND.
In order to calculate the feedback resistor values please consider that the BJT is used as current buffer:
VFB / R19 = (Vo - Vbe) / R18
hence:
R18 = R19 x (Vo - Vbe) / VFB
where:
VFB is the feedback pin reference voltage, for the LM2733 is equal to 1.23V (typ)
Vo is the output voltage
Vbe is the base-emitter voltage of the BJT
Best Regards,
Giuseppe
Hello Alan,
your schematic is fine. I don't think it is going to make a big difference if you put Cf1 directly to the FB pin or in parallel with R18.
You can try it and see how the output voltage ripple looks like during load transients then you can decide which one is better.
Regards,
Giuseppe