Hi,
We use the bq20z95 a few years on different configurations and PCB.
Last month we encountered an issue with floating temperature measurements. I monitor the temp values via bqEasy software.
I'll try to explain in details:
First I'm using external temp sensors.
When steady state (no chg/dsg current) the real value of temp is measured. Everything is ok.
But when starting discharge 10A at 25°C the temp value jumps to approx. 35°C, when 20A it jumps to approx 45°C.
When charging at same conditions (10A) the delta is negative, the temp jumps to 15°C.
At low currents there is also such phenomenon with relatively decreased values.
If internal temp sensor is used the temp jump is even extremely higher. At 25°C , discharge at 20A the temp jumped to 126°C
Do you have any idea?
Thanks,
Shlomi