This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Changing Data Flash variables in Z95



We are unable change the Min Lifetime Cell Voltage from 0 to 3200 and and min Lifetime Pack Voltage with our code. We have been able to unlock, lock the pack and read Manufacture Data. Do we have to do a Read All and collect all the Data flash data then change two variables and read write the flash data? Or is it possible just to change these two variables? We have captured a session from the EV2300 and the do a complete read of all registers and a complete write back. We don't have sufficient memory to do that. Can you help?

Mike