I can not save a *.senc file with the EV2400 and a Windows 7 computer. I can with a EV2300 and a window 95 system. I get a an "Error in reading flash: VB_UNKNOWN Flash content may be incomplete." A second screen appears "Error reading flash! Error code (decimal)= 100"
Using the same steps , unlocking the pack, placing BMS in ROM mode, READ TO A FILE. The same procedure works ONLY with the EV2300.
Any ideas?
Mike