Hi Everyone,
I need to power 4 IR LEDs that operate at a forward voltage of 1.5V and current of 100mA. Which LED driver should I purchase to provide the desired power to each LED?
One thing that I would like to have in a driver is easy product integration. I'm trying to build an IR camera and want to integrate these LEDs around the lens system, so I'll be soldering the LED wires to the chip by hand and securing them to back of the camera holding. I would also love to find a product that is already designed to operate at my desired current instead of manually altering the current with a resistor, if possible.
Thanks in advance for all your assistance and I look forward to your responses!
Best,
Michael