Hi,
I'm having trouble with TPS54231. It fails at CISPR22 class B conducted emissions. I can see a huge peak around 570KHz (switching frequency). It was tested with a custom board and also with TPS54231 evaluation module which is even worse.
This power supply is used directly on a 12V input and conducted emissions are directly measured on the 12V.
Do I have to systematically use an input filer (LC filter, common mode choke) ? I don't see any parameter I could change to improve it, since it's not an external mosfet that is used for switching.
Thanks in advance for your help!