Hi there,
I have a pcb where I would like to add an Arria 2GX125 FPGA. At present the pcb doesn't have the supply for the 0.9V rail.
I'm considering the TPS40042 using the design generated by SwitcherPro with Vin = 3.3V and Vout = 0.9V with Iout = 9A.
The pcb resides in a housing with no airflow & heatsink only and has a measured temp = 63.5 degC on the board. Can you tell me if I'm going to exceed the TPS40042 specs on junction temp/operating temp and go thru some power dissipation calculations relating to temperature. If there are any tutorials or background materials relating to DC/DC power calculations please forward.
Also, how high of an ambient or pcb temp can I tolerate above 63.5 degC before device shutdown or I violate the recommended operating junction temp?
Thanks,
Peter