Is it possible to bypass the WPC standard in any design with bq500110 series?
I also find the 5 mm limit is very annoying in most applications. I would like to have it transfer energy in 20-40mm range @ 1%-10% efficiency (10-50mA). From the file attached to this forum it seems physically possible. However, you said the WPC prevents this. Then is it possible to bypass the communication controlling the power output. For our design the energy efficiency is the least concern.
Thanks
Ling