This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Boost Converter

Other Parts Discussed in Thread: TPS40210, TPS61175

I am looking for an IC DC/DC Boost Converter that will take an input of 5 V and provide an output of 15-24 V. The output current is required to be at least 500 mA.

Please help!

  • Matthew, welcome to the forums.  I would like to ask that you put more information in your forum subject lines. This will help others in the future if they have a similar question.  One example would be to use “5V to 24V @ 500 mA boost needed” as the subject rather than just “boost converter”   More detailed subject lines are very important to help others know what the forum post is about.

    The power quick search at power.ti.com can help you select the right part for a given application.  Based on your specs, I would recommend the TPS61175 or TPS40210.

  • Chris,

    Thanks for the reply. I have chosen the TSP40120. I will make the subject headings more detailed in the future.

    Many thanks,

    Matt