This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq27541-v200 FCC and Qmax update

[1] Does the PassedCharge keep being integrated after FC bit is set?

[2] If [1] is yes, are FCC and Qmax increase on update timing?

[3] When charge is continued after full charge is detected, is FCC updated during charge?

     If FCC is updated, is Remain Capacity also updated to same value with FCC?

[4] Is FCC updated when FC bit is set? If it is true, how is it calculated?