We use the TPS65930 in our product.
Which is right in order to enable a COR function? [following 1or2 ]
TRM has the two following kinds of statements.
Respectively, logic is reverse.
1)TRM 4.4.2.1 COR Feature
The status register is cleared when its contents are read by the OCP bus. The COR feature is enabled by setting the <module>_ SIH_CTRL[2]) COR bit to 0. In this mode, the status register is cleared when an OCP read occurs. When the status register is read by OCP, a clearing pulse is generated to clear each bit
of the status register.
2)TRM Table 10-30. KEYP_SIH_CTRL
0x0: Clear ISR-specific bit field when write access mode.
0x1: Clear ISR when read mode.