This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Constant current source



Hello.

I'm quite inexperienced in this field and ask for advice and help.

I need to construct a constant current source, PWM controlled, input voltage up to 3 V. Required output current (by next component) should be up to 40 mA, so lets say that I would like that current source can generate 50 mA.

Can anyone suggest a component for this use or provide any additional information?

Regards,

BJ