Hai,
I am using a 7" TFT LCD in my design which needs TFT bias voltages. The voltages and their values are given below. It needs a specific power ON and OFF sequence which needs to be followed for long life of the LCD. I wanted to use TPS65105 as that provides the sequence required by the LCD. But the problem I am seeing is that the voltage generation delay between the voltages is not meeting the LCD requirements that is shown in the below diagram. Is there anyway that I can increase the delay between the voltages? But I am mentioning again that sequence is meeting. Kindly help.
I have attached the LCD Power ON and OFF sequence in the attached image.
DVDD - 3.3V - Generated by other DC-DC Regulator
AVDD - 9.6V - Generated by Vo1 output of TPS65105
VDDG - 18V - Generated by Vo3 output of TPS65105
VEEG - (-6V) - Generated by Vo2 output of TPS65105
VCOM - 4V - Generated by Vcom output of TPS65105
Regards,
Erfan