How does an NTC get connected to the bq51014? The bq51014 datasheet in figure 2 shows the NTC connected between TS-CTRL and ground. This more or less agress with the pin description of TS-CTRL. But in the "Simplified Block Diagram" the TS-CTRL pin is apparently a high-impedance input. Things are yet more confused by Figure 41 and accompanying text, which shows a network including VTSB (a pin that exists on other parts, but not on bq51014). The specifications table includes Vcold and Vhot which are percentages of Vts-bias (what's that?) and Vctrl thresholds for high and low. What's the function? hot / normal / cold? Or is it high / low? Is there in fact a curernt source at TS-CTRL? If it really is as simple as an NTC to ground, what nominal resistance and 'beta' should be used?