This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Defference betweenTPS659530 and TPS65950

Other Parts Discussed in Thread: TPS65950, TPS65930, TPS65921, TPS65951

Hi,

    Can you tell me about  the defferences between TPS65950 and TPS65950? Can I use TPS65930 to instead of TPS65950 about  USB.

  • TPS65930 is a depopulated version of TPS65950. The main difference is the package pitch 0.4mm for 65950 and 0.65mm for 65930.

    Please also note the current capability for VDD1 is higher on TPS65950 than 65930 therefore TPS65930 does not support the highest operating frequency. If it is needed consider TPS65950, TPS65951 or TPS65921.

    Datamanual for all these devices are available on TI.com.

    Please close the thread if it answers your questions
    Regards,
    Philippe