I am using a Sony SFH-1215B chemical fuse that has a max 15amp current. I want to make the pack larger 3s6p with a max of 22 amps. Can I put two SFH-1215B in parallel?
mike
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am using a Sony SFH-1215B chemical fuse that has a max 15amp current. I want to make the pack larger 3s6p with a max of 22 amps. Can I put two SFH-1215B in parallel?
mike
It's typically not recommended to use fuses in parallel. A slight resistance difference between the fuses can result in one fuse being blown and the other being only partially blown, which means you still have a discharge path. The best option would be to find a single fuse that can handle 22A.
I only know of the sony SHF1215B series of chemical fuses. They don't have any thing greater. Do you have a suggestion?
Mike
I don't have any suggestios, unfortunately. They are not typically available from distributors and we don't add fuses to any of our reference designs or EVMs. Your best bet would be to contact Sony.