For unstated reasons, it is considered dangerous to disconnect the battery from the bq78PL116EVM. To do so, one must press Shift-F2 (Safe Disconnect command) which invokes a popup that times out in 20 seconds. I'm finding it hard to disconnect all those wires from the EVM in said 20 seconds, especially due to having bare wires floating around that are connected directly to LiPo cells. Do I have to disconnect the wires in the opposite order of the required connect sequence? What am I missing here?
Bob