Hi All,
I am relatively new to all of this, and my understanding is only quite basic so please bare with me.
I am required to make a worst case analysis to determine if this voltage regulator is suitable for use in our intended application. I am wondering if anybody is able to assist here or point me in the right direction?
The specifications for the environment the regulator will be used in are as follows:
Regulator: TI LM2576S
Input Voltage: 11 – 16V
Output Voltage: 6.5V – 7.5V
Peak Current Draw: 1860mA
Max Current Draw: 350mA
Usage Temperature: -20 – 70degC
Package: TO-263
Is there any other information that would be required to create a worst case analysis? I guess we are wanting to be assured the voltage regulator will operate within its specification, while being used within our intended application as specified above.
Thank you for any assistance.
Danny