My apologies for posting this topic in two of the TI forums.
This one, related to the PMU's sees more appropriate that my original choice in the Sitara™ ARM® Microprocessors forum.
Sorry for that.
Here it is:
================================================================================
I have designed a board which is for the most part a "clone" of the ICE ( http://www.ti.com/tool/tmdxice3359 ) ,
with many other devices as required for our application.
The problem I am facing now is that the PMIC is not getting out of the "OFF" state.
The actual PMIC part is marked:
TPS65910A1
TI 1BK
CPQ9 G4
The most telling symptom is that Vref is stuck at zero Volt
( NOTE: measured that Pin 18 is not shorted to GND )
Other measurements are:
BOOT1= 1.8V ; BOOT0= 0V
0 V = SLEEP = NRESPWRON = INT1 = VDDIO = REFGND
1.8 V = VRTC = PWRHOLD
0.1 V = TESTV
5.0 V = PWRON = VCCIO
5.0 V = VCC1 = VCC2 = VCC3 = VCC4 = VCC5 = VCC6 = VCC7 = VBACKUP
Questions:
Is this the right PMIC for this processor ?
Any insight about what may be wrong?
Is there a document indicating how to actually bring up a board such as this,
with the procedures for flashing all the devices with the proper data so that the system will wake up ?
Thanks, Jure Z.