Hello everyone,
I've got a question on the registers of the bq32000 Real-Time-Clock. In the manual the whole registers of the clock are describted. There are also the initial values mentioned. The describtion says that all the reserved register values should be written to 0. But I found some registers that initial value of those bits were not zero (like TCH2 Register and CFG2 Register).
May somebody can tell me if this is an error in the manual or why these bits are not set to 0 automatically?
Thanks
Roldi