Hi,
I need to design +1.2V and +3.3V power supply circuits for my Xilinx Spartan-6 XC6SLX9-2CPG196C FPGA.
My design requirements are: VinMin = 4.0V, VinMax = 5.0V.
Output requirement is Vout1 = +1.2V, Iout1 = 550mA.
Output requirement is Vout2 = +3.3V, Iout2 = 650mA.
I'm looking for Smallest power supply solution.
Using TI Webench, it proposed me to use two LMZ10500 Switcher with following resistance value for Rt & Rb.
1. Vout1 = +1.2V, Iout1 = 550mA -> Rt = 80.6K ohms, Rb = 105K ohms
2. Vout2 = +3.3V, Iout2 = 650mA -> Rt = 80.6K ohms, Rb = 105K ohms
Wondering if LMZ10500 Switcher is the best option that i can use? Please help to propose if have any newer devices.
Thanks.
Regards,
Atthen