All,
I am in the process of developing a battery charger for Li-ion, NiCad, and NiMH battery chemistry. I wanted to include gas gauge functionality into the charger, but was unclear as to what my available options and corresponding best choice would be. One complication is that the batteries are composed of 4 series stacked cells, but the charger only has access to the serial terminal voltage, and not the individual cell voltages. I was thinking about using the BQ20Z65-R1 for its accuracy with Li-Ion, but wasn't sure if this could also be used with the other chemistries, or how he performance would be if the individual cells are not monitored. If this is not a good option, it appears I would have to use a multi-chem chip like the bq2060A. Any advice in this area is appreciated.
Thanks, Troy