Hello everyone!
I have built a boost converter based on TPS61220 to power a circuit from a battery. I have been testing the converter alone and encountered a problem.
With input voltage of 3.7 V and output voltage of 5.5 V, the datasheet specifies I would get output currents up to slightly below 200 mA (the spec is actually for 5 V output). However, my converter provides only 11 mA, and increasing the load causes the output voltage to drop. This is not enough for me.
I have examined the input and output voltages - the ripple is no more than 40 mV at the input and 50 mV at the output. I have also looked at the inductor current, and saw the strange behavior there: the converter operates in short bursts. The bursts last for no more than ~15 switching cycles, followed by quite long periods of idling. This would have been OK for low loads, but this also happens at overload. The bursts themselves look good, with clean sawtooth-like inductor current peaking at around 300 mA.
I have tried to increase input capacitance, with veery slight improvement. I have replaced the IC with another one, and still get the same results.