Hi, I've some question about the specification of the bq24040 (http://www.ti.com/lit/ds/symlink/bq24040.pdf).
- Page 4 : Iout : 10mA to 800mA; on the same page are presented the KIset factor from 10 to 800mA.
- Page 7 : Range is 10.8k (50mA) to 675 Ω (800mA).
Which one is true? minumin fast charge current is 10mA or 50mA?