I'm using the UCC27322D mosfet driver. It's output is rated for a peak amerage of 9 amps. I've been bench testing one for a number of hours, and just now smoked it. I mean it was glowing cherry red before I turned it off. But it has worked just fine for about 6 or 7 hours so far. When I put a laser temp sensor on it after a couple of hours, it was reading at like 85F or so. Barely warm to the touch.
Now, this may be the stupid part, but I'm driving 6 mosfets with it. Theoretically that shouldn't be a problem, but maybe that's the whole problem. 
Here is the schematic. Vdd is 12 volts. F1-F6 are fuses, which I'm using on the prototype just to be able to isolate 1 or more of the FETs during testing. The FETS are International Rectifier IRFB4310ZPBF.
Now, what you don't see in this schematic is the fact that I'm getting some big pulses back to my mosfets. I get 75 volt spikes across my source and drain pins on the mosfets, for every output pulse. When I scope the power to the driver, or the input or output pulses to and from the driver, I don't see any of these spikes getting to the driver. Both the mofet gates and the driver input/output lines are very clean. So, while I don't see how the spikes can be bothering the FET driver, this data needs to be included here.
Is it just stupid to drive so many FETs with one driver? On paper, it seems fine, but then, on paper my FET driver didn't glow cherry red.