I am going to use BQ24610 for Li-ion charging. Can you please guide me about the working of the EVM board. if there is any datasheet in which each step is clearly shown how to perform the Task.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am going to use BQ24610 for Li-ion charging. Can you please guide me about the working of the EVM board. if there is any datasheet in which each step is clearly shown how to perform the Task.
Are you talking about HPA422 document? Load 1 is connected to system to simulate the system load. So, it can be an electronic load or resistor load. Load 2 is connected to BAT output to simulate a battery. So, Load 2 should be an active load which can source or sink a current.
LOAD #1
30V (or above), 5A (or above) electronic load that can operate at constant current mode
LOAD #2
Kepco bipolar operational power supply/amplifier, 0 ±30V (or above), 0 ±6A (or above).