I am using Bq24610 for charging Li-ion battery. In the EVM of Bq24610 We require 3 power supplies and 2 loads. But Traditionally in charger circuit we can use only 1 power supply for input and we can use output for battery charging. Please tell me reason for the same.
Power Supplies
1. Power Supply #1 (PS#1): a power supply capable of supplying 30-V at 5-A is required.
2. Power Supply #2 (PS#2): a power supply capable of supplying 5-V at 1-A is required.
3. Power Supply #3 (PS#3): a power supply capable of supplying 5-V at 1-A is required.
Load
1. A 30V (or above), 5A (or above) electronic load that can operate at constant current mode
2. A Kepco bipolar operational power supply/amplifier, 0 ±30V (or above), 0 ±6A (or above).