This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Regulation problem with tps84410

Other Parts Discussed in Thread: TPS84410

I am using the Tps84410 adjustable regulator to generate +3.3V from a 5V input. I've used the the datasheet to calculate the adjustable resistor in order to set the output to 3.3V. I chose Rset as 459 and Rrt as 348k resistor values so that Vout = 3.3v.

I used all the other suggestions from the datasheet as well for the other discrete components in the circuit and followed the layout design guide down to the letter. My concern is that when the regulator has no load it regulates the 3.3V but when we place the regulator under load (around 4A) the output drops by approximately 120mV.

This 120mV drop under load seems too much of a drop.

Do you have any ideas as to what might be going on?