This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

pwm generater

Hi,
We are looking for other solution of the pwm generater, all we need is:
300 or 600 HZ pwm with duty cycle ratio >1000. eg, 300HZ, min high of the PWM should be less than 3.3ms/1000= 3.3us
max could be less than 50%. as long as it can give me min 50%/1000, we are OK,
digital input is fine (we could put ADC), but no micro nor FPGA, this is a must.
thanks
Frank