i have made tps61087 ic based dc-dc converter.
input range is 2.5V to 5V and output is 18V / 200mA.
when i give input from Duracell(two cell in series to make 3V) or 5V from CPU-SMPS dc -dc is working fine.load taking 100mA in working condition.
but when i give input 3.3V from SMPS, output is 18V in open condition.when i connect load voltage become 14V-15V and load is not working.
please help me to solve this problem.