This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A4001 Extended temperature operation less than -40degC

Other Parts Discussed in Thread: TPS7A4001, TPS7A4101

Hi,


TPS7A4001 suits our requirement other than the operating temperature range.

Do you have any test data for the extended temperature range from -40degC to -48degC ambient?

What will be the issue if I try to operate TPS7A4001 at -48degC ambient?


I am looking for a linear regulator with following specification,

Vin= 18.5V to 32.5V

Input surge= 45V

Vout= 5V

 Iout= 10mA

Operating temperature range= -48degC to +93degC

Can you please suggest any linear regulator which can satisfy our requirements?


Thanks

Shihab.