hi i have problem with dell d620 batterys having bq2084 ic in it. these batteries are not charging at all or charging upto certain extent say 60% 80% 90%.while discharging some of these batteries drops to zero from 50% 35% 30%. shuts down laptop. can u have any suggestion in this regard
thanks