With both the 5926 and 5917 (and others) each "out" pin can sink up to 120mA; so for the 5926, this add up to almost 2Amps. Question being, where does all of this connect back to the GND net? Is all of this current going through the single GND pin, ie. this pin's trace back to the power source GND needs to be capable of handling 2Amps? And/or should the powerpad be connected to GND as well?