This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Fusion Digital Power Designer

Guru 13485 points
Other Parts Discussed in Thread: UCD9246, UCD7242

Customer ising UCD9246 +UCD7242and  the Fusion Digital Power Designer,  and when configuring one output to 1.05V and the other to 3.3Vthey got a fault of “Power_good#”.

Vin is 12V.

Its dose not happened ,when they used 2 “close’ outputs like 1.5V and !.8V!!!

Can you help were is the problem?