Hi,
I have some problems with the two-Phase Interleaved CCM PFC Controller -UCC28070-
1 Observation : in the starting phase, during the soft start, the impulses start
on both channelssimultaneously, and at a certain moment a double impuse
is applied to one channel and saturates the coil, by producing a short-circuit.
Questions :
1. Why the impulses do not start in antiphase?
( after the soft-start phase, the impulses are shifted correctly)
2.What shall be done, so that the impulses shall remain in antiphase during the soft-start?
Tks,