This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

need a recommendation controller/topology to design a non-isolated 400Vdc to 30Vdc with output current = 14 Amps

Other Parts Discussed in Thread: UCC28950

The requirement for a non isolated DC-DC converter input_output ratio is high. What I need is a recommendation of choosing the controller and topology. The controller include I limit and soft-start features.

Vin = 380-420; Vout = 29

Iout = 13A