We have a 6kW UCCC28070-based PFC supply. Vout is 403Vdc, and it should operate throughout the full universal input range.
At 160Vac and above, it will deliver 6kW stably. At 120Vac and below, power drops off because Vout sags. I can only deliver ~5kW @ 120Vac. After a burst of @ 5.5kW for a couple seconds, Vout falls to ~380Vdc and the power drops.
If I trigger my scope on Vout falling to 380V, I see that the CSA and CSB pins are completely below 3V. The duty cycle is ~50%. So it doesn't appear to me the UCC28070 is pushing the supply as hard as it can to maintain a regulated Vout. The traces are as follows: Yel - PFC Vout, Cyan - CSB, Mag - Vac, Grn - Iac.
The max duty cycle clamp is set to 95%. I adjusted the voltage going to CSx and PKLMT to no avail.
What could prevent the controller from cranking up the duty cycle and/or allowing higher FET current once Vout has fallen out of regulation? Because this is line voltage dependent, it seems like there's a power limit somewhere in the system.