This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65910



1)      According the Table 6, there should be 500-550usec delay between the PWRON signal going LOW and the INT1 pin activating.  We are seeing ~500msec.  Was this a typo in the datasheet? Or are we not setting something up properly?

2)      Our desire and understanding is that INT1 pin interrupt can be activated by a falling edge on the PWRON pin.  However, if we keep the PWRON pin LOW after the initial transition and we acknowledge the interrupt, INT1 is re-activated.  Which suggests it is not edge triggered but level triggered.  Which behavior is correct?