This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ouput of LM25007 become unstable under certain conditions

Other Parts Discussed in Thread: LM25007

Hi,

My name is Henry. I'm using LM25007 as power source to supply a heater(the heater is a 25 ohm resistor), input voltage of LM25007 is 24V, output voltage is 7.5V. there is a PWM signal to control a PNP transistor to on/off the power to the heater. I tried the PWM signal with frequency of 1KHz and 2KHz, everthing is OK.

Until I use frequncy of PWM to 500Hz, 250Hz or 125Hz, the output of LM25007 becomes regually up and down. the  voltage can drop for several volt and can recover gradually. 

Does anybody has experience with this?

Thanks for your attention!

 

Henry Li