Hello all,
I'd welcome some input please if you'd be so kind. I have a system running the above part and the system works operationally however the individual cell voltage readings are really quite strange.
I have a two cell system and am reading an overall voltage of (say) 7700 mV although the cell voltages read as 3331 mV and 4433 mV (cell 1 and cell 2 respectively). This is simulating a battery with two 1% precision resistors.
If you need any further information, I'll happily provide it but I think it may be a calibration setting which I have overlooked or something that others may have seen in their own development. But any ideas would be most appreciated.
Kindest thanks.