I am looking for an application note or some suggestions to add load sharing capability to the LM5017. I have the need to add some redundancy to my power supply using two of these devices. The reason that this device is selected is that I am looking for a simple solution that can handle input voltages higher than 80V.